AXIS#.GEAR.MOVE

Description

The command AXIS#.GEAR.MOVE starts the electronic gearing procedure according to the selected electronic gearing mode. The electronic gearing process can be stopped using the AXIS#.STOP command.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5503

1

5503 (0x157f)

AXIS1.GEAR.MOVE

Unsigned8

Read/Write

No

71039

2

5503 (0x157f)

AXIS2.GEAR.MOVE

Unsigned8

Read/Write

No

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.GEAR.MOVE

5503

Unsigned8

Read/Write

-

Related Topics

Electronic Gearing